A user opens an assembly in Design Manager and sees colored icons are in front of the file names. Some of these icons have a red or blue shade on the icon, others have blue text. What do these icons mean?

Solution
Icons with a blue shade indicate a link originating from an Assembly Copy feature.
Icons with a red shade are an Assembly Copy feature.
Blue file names occurs when multiple occurrences of the same file are shown on the same level. We set the color to blue to indicate the line has NOT been expanded. We do this for performance and space reasons; you can expand the line manually.
See the Solid Edge Help documentation for more information:
http://docs.plm.automation.siemens.com/tdoc/se/110/se_help#uid:xid1129777:xid13
29553:index_xid1329825:xid1169613:xid1175782:xid1174901Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: DESIGN_MANAGER
Ref: 001-9131172