Unable to change properties of Std Parts

2021-10-06T23:52:01Z

Summary


Details

Now that Standard Parts are generated with a 'released' status, you are unable 
to change the properties needed to show in Parts Lists. How do you change the 
behavior of Standard Parts so they are 'available'?



Solution

For existing Standard Parts that are set to 'released' use the Data 
Preparation utility delivered with Solid Edge to change the status of ANY 
Solid Edge file...


- open the Data Prep utility 
- select Unmanaged/Insight at the top 
- click [Select file/Folders] and select the top-level folder of the files 
- generate import list --> creates an Excel spreadsheet 
- after the spreadsheet appears click on the SE Data Prep tab 
- click the Set File Status button 
- click the [Available] button 


Once the operation is finished you can close without saving.


To prevent any newly generated Standard Parts from being set to 'available' 
you can add a registry switch.


- run REGEDIT.exe 
- browse to HKEY_LOCAL_MACHINE\SOFTWARE\Unigraphics Solutions\Standard Parts 
- add a registry key "ReadOnlyFlag"="True" as a string value


Afterwards, any NEW parts will be generated with a status 'available', but 
with the "read-only" flag enabled.



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 732SP1
Product: SOLID_EDGE
Application: EXTERNAL_APPS
Version: V110.0
Function: STANDARD_PARTS

Ref: 001-9126101

KB Article ID# PL8003965

Contents

SummaryDetails

Associated Components