Part attributes which are linked to an expression break after the item is reloaded.
Solution
Set attribute mapping /master=cad for that specific attribute.
The attribute mapping of a NX part-attribute which is linked to an expression
is expected to be driven from the NX expression value. TC-attribute should not
overwrite this value from TC into NX anymore. Therefore the mapping for this
attribute should have set the switch /master=cad . This prevents that the
TC-attribute overwrites the NX-part-attribute value and breaks the link to the
expression.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: ATTRIBUTES
Ref: 001-9110731