NX NX: Order of installation for NX patches?

2021-10-06T23:26:18Z
NX System Administration

Summary


Details

What is the order of installation for a fully patched install of NX?

Solution

For installations prior to NX 12, you should begin with the base installation. 
We'll use NX 11 in this example. First install NX 11, Next install the MR NX 
11.0.2. And finally install any MP, for instance NX 11.0.2 MP 07.


Beginning with NX 12, MR's will be full installations. For instance, if you 
want to run NX 12.0.1, you no longer have to first begin with NX 12. You can 
install NX 12.0.1 directly, as this is now a full installation. 

Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2003_SP2
Product: NX
Application: SYSTEM
Version: V11.0.2
Function: WNT_INSTALL

Ref: 001-9124819

KB Article ID# PL8003944

Contents

SummaryDetails

Associated Components

Installation Licensing Plotting