Siemens PLM Licensing NX: Vendor Daemon is down?

2021-10-06T23:26:18Z
Licensing Maintenance

Summary


Details

A virtual machine crashed bringing down the license server; a new virtual 
machine was built using the same mac address as the original machine - however, 
the vendor daemon fails to start? 

Solution

This happened because the CompositeID is made up of more than just the mac address. 
Other hardware identifiers are used in the calculation that makes up this id. 
A new license file will have to be generated based on the new composite id. 

Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: SYSTEM
Version: V12.0
Function: SYSTEM_TOOLS

Ref: 001-9124671

KB Article ID# PL8003942

Contents

SummaryDetails

Associated Components

Siemens PLM Common Licensing