Tecnomatix Cannot initialize Nachi RCS

2021-10-07T00:01:20Z
Process Designer

Summary


Details

Error:  "The RCS could not be initialized:  Allocation problem:  No more memory.  (0)"
Error:  "RCS_MA~1.exe has stopped working".
           "A problem caused the program to stop working correctly".  
           "Windows will close the program and notify you if a solution is available".

With Robot / Visible Shell enabled, you will see this error:  "No such file of directory.  'touch' is not recognized as an internal or external command, operable program or batch file".

Solution

The RCS is looking for a specific folder to write in and cannot find it.
Make sure there is a 'TMP' folder in the root of drive 'C'.  If there isn't, it will generate all the errors listed above.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANNING_APPLIC
Version: V14.0.2
Function: PROCESS_SIMULAT

Ref: 001-9119737

KB Article ID# PL8003937

Contents

SummaryDetails

Associated Components

Planning Logistics