Details
Using Edit --> Properties --> selecting a cylinder then selecting the General tab has the option to edit the Feature Name. How can you add an Object Name?
Solution
Depending on what is selected will determine what Properties dialog is opened.
Selecting the Cylindrical Feature opens the Cylinder Properties dialog and Feature Name is available.
Selecting the Solid Body of the Cylinder opens the Solid Body Properties dialog and Object Name is available.
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: SYSENG
Version: V10.0
Function: DISPLAY
Ref: 001-9035064