Generate a derived curve between non-identical splines.

2021-10-06T23:26:18Z

Summary


Details

Interpolate or Derive a Curve Between Two Spline Geometries in Modeling.


Solution

This should generate a precise derived curve between the two different spline
paths.

1. Create a line connecting the nearest ends of the splines and use "Swept" to
follow the two splines as guide curves.

2. Create 1/8" or 1/4", length is unimportant, long line segments
perpendicular to the step 1 line segment with the mid-point at the end of each
spline. This creates a total of two linear segments.

3. Use Swept on the two, step 2 linear line segments along each splines length.

4. Create a Midsurface between the two surfaces created in step 3.

5. Create an Intersection Curve between Midsurface (step 4) and Swept surface
(step 1).

A less precise method that may fail to be accurate at any portion along the
Swept guide curves method.

Generate a Swept line from the Mid-Point of a line connecting the two ends of
the splines on one end.

While this will work, it can deviate and will be less precise than the
recommended precise procedure.


Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V12.0.1
Function: FREE_FORM_MODEL

Ref: 001-9121877

KB Article ID# PL8003892

Contents

SummaryDetails

Associated Components