What is the format / syntax used for the Ribbon toolbar files and other menu
related configuration files?
Which files should be modified to create customized ribbon toolbar interface?
Solution
The documentation contains full details of this, however it can be difficult
to find as it is not referenced directly within the main help menu.
It is found in the Programming Tools Section:

Then under the section "Menuscript User's Guide".


Within the guide are many examples of how the menu files can be modified and the syntax that should be used.
Notes and References
https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_api#uid:index_menuscript
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V12.0
Function: UI_TOOLS
Ref: 001-8368361