How to add prefix in smart dimensions without dia symbol?

2021-10-06T23:51:57Z

Summary


Details

The basic requirement here is to add "PCD" as a prefix for all dimensions but when you use the prefix option in dimensions the PCD comes along with DIA symbol.
If you have requirement where Dimension value should come after the text PCD without dia symbol (Ø) . 
For example if prefix option is used the output would be "PCD Ø50" but requirement is "PCD50". 




Solution

You can suppress diameter symbol from Dimension properties.
Steps:


- Select the dimension


- RMB (Right Mouse Button) click > Select 'Properties'


- Select [Terminator and Symbol]


- Check select Suppress diameter


It suppresses the diameter symbol on diameter dimensions placed with the Smart Dimension command.


- Click [OK]

Notes and References

9110424

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: DIMENSIONS

Ref: 001-9110424

KB Article ID# PL8003775

Contents

SummaryDetails

Associated Components