The "C" is not displayed with the chamfer dimension in drafting

2021-10-06T23:26:16Z

Summary


Details

The "C" is not displayed with the chamfer dimension in drafting.

Solution

To edit existing chamfer dimensions:
  1. Highlight the chamfer dimension, 'MB3-->Settings'.
  2. Select 'Prefix/Suffix'.
  3. Toggle Location to "Before".
  4. Set the Text to:  C
To set the preference for future chamfer dimensions:
  1. In the Menu, select 'Preferences-->Drafting'.
  2. Expand 'Common' and highlight 'Prefix/Suffix'.
  3. In the Chamfer Dimension group, set Location to "Before" and set the Text to:  C
  4. OK the Drafting Preferences dialog.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0.3
Function: DIMENSION

Ref: 001-9095038

KB Article ID# PL8003726

Contents

SummaryDetails

Associated Components