Simcenter 3D Solutions Error message in the FEM: Imbedded object cannot be deleted in isolation.

2021-10-06T23:26:16Z
Simcenter 3D

Summary


Details

If a node is selected to be deleted, in the FEM, and the following error message displayed message is:  embedded object cannot be deleted in isolation, the following scenario may be the reason.

Solution

Often,  nodes cannot be deleted if they are attached to elements, loads or constraints.  However,  they can be attached to other objects that will also prevent that node from being deleted.  Sometimes it may be more difficult the find the associated object.  In this example,  listing the node to be deleted did not list any connected elements.  The idealized and Master Part were not active in the FEM so they were loaded.  Once the CAD geometry was loaded,  the node could be deleted.  It  turned out that the node had been associated to a polygon edge by a 1D connection and the CAD geometry had to be loaded before the node could be deleted.

Notes

KB Article ID# PL8003679

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow