Want to update model once I finish modifying dimension.

2021-10-06T23:51:51Z

Summary


Details

Is there any setting by which user can stop/postpone the model update till he complete all dimension changes. 



Solution

Automatically updates information in the working environment when Automatic Update is on. When Automatic Update is off, changes are postponed until you select the Update Relationships command or the Update All Relationships command.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: APPLICATION
Version: V109.0
Function: OTHER

Ref: 001-8994425

KB Article ID# PL8003661

Contents

SummaryDetails

Associated Components