Take a measurement and build a formula while moving a component in NX11.

2021-10-06T23:26:16Z

Summary


Details

In NX11, when moving a component, where is the option for Measurement Distance?  In previous versions the measure distance icon can be selected at the bottom of the Expression Editor. 



Solution

In NX11, after selecting a component to move, pick the down arrow next to the Distance entry field and select Formula. The new Expression editor opens with an active cell to enter a value. But if you pick outside the active cell it will no be longer active, then use MB3 in the cell and select Edit. This will open the Edit dialog where you can select the icon for Measure Distance and build a formula from that measurement.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V11.0.2
Function: POSITIONING

Ref: 001-9096703

KB Article ID# PL8003649

Contents

SummaryDetails

Associated Components