Solid Edge Edit Links replace source file is too large

2021-10-06T23:51:51Z

Summary


Details

When replacing part ( with Insight managed data) receive message:


Change Source 
 <filename> 
 The file size exceeds the limit allowed and cannot be saved. 



Solution

The issue is caused by a Microsoft default regestry setting. MS will not 
allow a file larger than 50MB to be download from a website.


This problem is caused by a download file size limitation.


'FileSizeLimitInBytes' is set by default to 5000000 which limits the download 
on the client side.


The problem is solved by modifying the Registry Parameter: {ON THE CLIENT}


HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\WebClient\Parameters 


1. Select 'FileSizeLimitInBytes' -> RMB Modify... you will see the Default 
Base: Hexadecimal - Value: 2faf080 then change this to Base: Decimal - (Display 
of the value is now in Bytes) 
2. Change Value to 104857600 Bytes (=100 MB , maximum is 4294967295 which is 
4GB) 
3. Reboot



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109.0
Function: INSIGHT

Ref: 001-9094356

KB Article ID# PL8003645

Contents

SummaryDetails

Associated Components