Synchronize component layer display on drawings

2021-10-06T23:26:15Z

Summary


Details




Set Layer display in the drawing file to be the same as the master model assembly part easily. 



Solution

This can be accomplished by selecting the master model assembly file and using MB3 --> Properties --> Assembly tab --> Synchronize Subassembly Properties --> Layers. The layers displayed in the drawing file should now match the assembly file.


From the NX docs: 

Sets the properties of each subassembly component to be the same in any assembly that the subassembly is used in. Layers, Display, and Attributes take their settings from the equivalent components in the selected subassembly, as if that subassembly were the displayed part. The settings are applied to the same components in the displayed part.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: GATEWAY
Version: V11.0
Function: LAYER

Ref: 001-9093485

KB Article ID# PL8003620

Contents

SummaryDetails

Associated Components