Custom symbol does not display when inserted into a Tabular Note

2021-10-06T23:26:15Z

Summary


Details

Custom Symbol will not display after adding it to a Tabular Note cell. 



Solution

The Tabular Note table could be from a previous version of NX and will need to have the 'Version Up' tool applied to it in order for the custom symbol to display.


Applied the following procedure to the Tabular Note table:
  1. In the Menu, select 'Tools-->Version Up'.
  2. Select the Tabular Note table.
  3. OK the Version Up dialog.

Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: SYMBOL

Ref: 001-9086546

KB Article ID# PL8003573

Contents

SummaryDetails

Associated Components