Simcenter 3D Solutions Export of Adams solver input file is not available

2021-10-06T23:26:15Z
Simcenter 3D

Summary


Details

Why is the "Adams Solver Input File" Export option unavailable (greyed out) 

for Simcenter Motion 11 or 12 users? What options are available to export a 

file from Simcenter Motion to import into Adams View? 

Solution

The "Adams Solver Input File" export option is only available for some 

academic licenses that have the Adams solver for Simcenter Motion. The 

Recurdyn "ADM" translator should be used in lieu of the "Adams Solver Input 

File" translator. The "Adams Solver Input File" translator generates an ANL, 

CMD, and TXT file. The "ADM" translator generates an ADM, CMD, and TXT file. 

When importing the CMD file into Adams View, both sets of files will produce 

the same result. 

Notes

KB Article ID# PL8003534

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow