Currently when creating a cylinder, there are 14 facets or sides to make the circle.
Considering the diameter (30mm), it is very rough and not accurate when trying to find collisions with the cylinder.
How can the number of facets that make a cylinder be controlled?

Solution
In the Options, change the General / Geometric Modeling / Approximation Tolerance from 0.5 to a smaller number, such as 0.1.
It will resolve the issue.


Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANNING_APPLIC
Version: V13.1
Function: PROCESS_SIMULAT
Ref: 001-9080876