Details
Steps to reproduce
-----------------------------
1. Create a new part file.
2. Create two bodies.
3. Execute "Radius" command.
4. Select one face of the body – Apply.
5. Hide the created feature.
6. Execute "Radius" command again.
7. Select the other body face.
-> The feature will be overwritten.
If we select a face using "Radius" command and hide the feature created by executing it, then select another face using the "Radius" command again, the feature will be overwritten.
If it is not hidden it will be added to the feature.
Radius/Distance/Slope/Reflection all exhibit similar behavior.
Question.
---------------
1. Is this working as designed?
2. If designed, let us know the reason.
Solution
A1. This is working as designed.
A2. When Radius Analysis is already created, and it is not hidden. In this case, when the reflection dialog is launched, the faces upon which Radius Analysis was applied are picked up. Then, any further selection adds those to those that already had radius analysis.
When Radius Analysis is already created, and it is hidden. In this case, when the reflection dialog is launched, the faces upon which Radius Analysis was applied are not picked up (because user has specifically hidden the Radius AO). Then, any further selection adds the selected objects to a list that had no faces to begin with.
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V11.0.2
Function: INFO_ANALYSIS
Ref: 001-8989445