NX How to disable Summary tab in ANT when Active Workspace is installed

2021-10-06T23:26:14Z
NX for Design

Summary


Details

By default in NX 11 summary tab is available when active workspace is installed.
When summary tab is selected by the user, NX tries to display all the properties due to which customer is facing performance issue



Solution

To disable the summary tab set the following environment variablele variable 
 
set UGMGR_ANAV_ENABLE_SUMMARY_WEBAPP_COMP=FALSE








Notes and References

9028818





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: ACTIVEWORKSPACE

Ref: 001-9028818

KB Article ID# PL8003475

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX