Details
Pop-up window that says "There is an update available: 13.2.3, Do you want to download the update".
We do NOT want our users updating their software, and need to disable this version check.
Solution
Here is a modification you can do in the registry. Under the key 'HKEY_CURRENT_USER\Software\Tecnomatix\Tecnomatix Plant Simulation 13.2' there is a DWORD value with name 'UpdateCheckDate' which contains the time of the last check.
If there is a value there, delete the entry.
Next, look for this DWORD in 'HKEY_LOCAL_MACHINE\Software\Tecnomatix\Tecnomatix Plant Simulation 13.2'.
Set this value to a high value like 100000.
This modification is not recommended if you are not familiar with the registry or how to modify it.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V13.2
Function: LOCALIZATION
Ref: 001-9072459