Turning OFF History-Free mode in the part navigator for NX11.

2021-10-06T23:26:14Z

Summary


Details

Transitioning from NX9 to NX11 the part navigator displays all of the objects 
as Solid Bodies and Timestamp Order is not listed as an option from MB3. Need 
to changing it so the that objects display as features.



Solution

At the top of the Part Navigator, there is a History-Free Mode option listed 
that needs to be changed to History Mode. Select on the History-Free Mode and 
Right Mouse Button and select History Mode.Select OK to the Modeling Mode 
Alert, then notice that the History Mode setting will be removed and the Solid 
Bodies now display as "Bodies" and new features will display as features.


The part file MUST be saved to keep the part in History mode.


History Free Mode has been retired in NX11, refer to the NX11 Release Notes 
for more information. 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V11.0
Function: PART_NAVIGATOR

Ref: 001-9076621

KB Article ID# PL8003437

Contents

SummaryDetails

Associated Components