Can you change the language interface to French on a English OS machine?

2021-10-06T23:51:43Z

Summary


Details

Is there a way to change the language interface to French on an English operating system 
machine.



Solution

There are two things that you have to do and they are as follows:


1) Go to the Solid Edge Options then to the Helpers tab and scroll to the 
bottom to Language and uncheck the "Use English in the user interface" option


2) Go to the Windows Control Panel then to the Clock, Language and Region 
settings then to the Format tab and change to the desired Format that you are 
wanting. 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2012_R2
Product: SOLID_EDGE
Application: APPLICATION
Version: V110.0
Function: UI

Ref: 001-9076460

KB Article ID# PL8003436

Contents

SummaryDetails

Associated Components