How to improve the resolution of non-linear edges in keyshot?

2021-10-06T23:51:43Z

Summary


Details

How to improve the resolution of non-linear edges in keyshot? 



Solution

If a KeyShot render file created from Solid Edge contains edges that are not 
smooth, the KeyShot geometry was most likely created with medium or low 
resolution.


To improve the resolution of the geometry, you can change an option in Solid 
Edge and update the KeyShot file. 
First open the KeyShot file and then the Solid Edge file which the KeyShot 
file was create from.


The option to increase the resolution of the Keyshot geometry is located in 
Solid Edge under the Tools tab> KeyShot> KeyShot Options. 
In the KeyShot Options dialog box, increase the Output Quality to High 
Resolution and updated the KeyShot file by clicking KeyShot Update or KeyShot 
Render. The geometry should update in the KeyShot file and the edges should 
look smooth as expected.



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: EXTERNAL_APPS
Version: V110.0
Function: KEYSHOT

Ref: 001-9075533

KB Article ID# PL8003434

Contents

SummaryDetails

Associated Components