How to exclude certain custom NX attributes from being transferred to JT?

2021-10-06T23:26:14Z

Summary


Details

Have turned on all attributes in NX to be transferred to JT upon an export by 
setting "getAttributes = true" in tessUG.config. 
The NX part file also contains attributes that should not be shared when the 
JT is generated. 
Is there a way to specify which attribute(s) should not be transferred to the 
JT file?



Solution

If you for instance have the custom attribute "my_hidden" defined in NX with a 
value, you can exclude it from being transferred to a JT file by defining: 
------------------------------------------------------- 
Filter { 
 MetadataKey = "my_hidden" 

------------------------------------------------------- 
in your tessUG.config file. 
(The Filter section in the tessUG.config would normally be after the 
"EAITranslator" section)



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: TRANSLATOR
Version: V10.0.3
Function: NX_JT

Ref: 001-9073834

KB Article ID# PL8003425

Contents

SummaryDetails

Associated Components