NX Shop documentation - mom variables not available

2021-10-06T23:26:14Z
NX for Manufacturing

Summary


Details

Various mom variables are not available for use in Shop Documentation

Example: mom_oper_program

Solution

This is documented limitation:

Home > Manufacturing (CAM) > Manufacturing General > Shop Documentation >

Customization on Output Format

MOM variables are dynamic, and change based on the operation. They may be

added or changed with each release.

Note

Some variables related directly to the tool path are available only during

postprocessing, and are not available in Shop Documentation. If you need to

use these, you should use the postprocessor to generate your shop

documentation.

Notes

KB Article ID# PL8003423

Contents

SummaryDetails

Associated Components

Manufacturing General