In Hole Table; how to change hole numbers like 1, 2, 3 instead of 1.1, 1.2, 1.3?

2021-10-06T23:51:41Z

Summary


Details


In Hole table the Hole numbers are appearing as 1.1, 1.2, 1.3 and so on.
User wants to see Hole number simple numbers as 1, 2, 3 etc.

Solution

Steps: 
1. Select the Hole table
2. Right Mouse Button Click > Select Properties
3. Use the Options tab to specify whether you want to see hole origin or hole number in the first column of the hole table. 
4. Clear/ Uncheck the option 'Show origin or group name in list'
- When this option is cleared, the group designator and delimiter are removed from the Hole column and from the hole callout annotation.

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: TABLES

Ref: 001-8543029

KB Article ID# PL8003398

Contents

SummaryDetails

Associated Components