A CAM program was created to mill a Part Family Member. That program file was then copied and the member switched using Replace Component. Will that CAM program update automatically if the Part Family Member is replaced with another?
Solution
Yes, NX will automatically update the geometry in the operation. All that is required is to regenerate. The Replacement Assistant is not needed to re-associate the geometry.
Notes