How to create an english units Hole Table from a metric part file

2019-04-18T18:54:45Z

Summary


Details

How to create an english units Hole Table from a metric part file.



Solution

The Hole Table will be reported in the units of the drawing. To change the units of the drawing: 
  1. In the Part Navigator, highlight the drawing sheet and select 'MouseButton3-->Edit Sheet'. 
  2. On the Sheet dialog, in the Settings group, specify the units to display the Hole Table.
  3. OK the Sheet dialog. 
  4. Add the Hole Table to the drawing and it will display in the drawing units. 
  5. To use the same units for dimensions, in the Menu, select 'Preferences-->Drafting'. 
  6. On the left, expand 'Dimension-->Text' and highlight 'Units'.
  7. On the right, set the Units for the dimensions to be displayed.
  8. OK the Drafting Preferences dialog.



Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: TABLES

Ref: 001-9062165

KB Article ID# PL8003319

Contents

SummaryDetails

Associated Components