How to make Datum Planes clear without any color.

2021-10-06T23:26:13Z

Summary


Details

Make Datum Planes Clear or Transparent without any Shaded Translucency



Solution

Turning off the translucent shaded Datum Plane display can be done by checking 
the box in NX11 for 'File -> Preferences -> Visualization Performance -> 
General Graphics (tab) -> "Disable Plane Translucency" '.  This works only 
during the current NX session.


This can be permanently turned off per user by selecting 'File -> Utilities -> 
Customer Defaults -> Gateway -> Visualization -> Performance (tab) -> General 
Graphics (group with blue text) -> (check box) "Disable Plane Translucency" '.


Here is the description from the NX documentation:


Disable Plane Translucency

Controls whether datum planes are displayed with translucency.  If this check 
box is not selected, and if the view rendering style is not Static Wireframe, 
the datum plane is filled with translucency.  If the check box is selected, or 
if the view rendering style is Static Wireframe, only the perimeter of the 
datum plane is displayed.

Display performance can be degraded if many translucent datum planes are 
displayed. Select this check box if performance is unsatisfactory while 
translucent datum planes are displayed. 

Disable Plane Translucency is a session option, so it applies to views in all 
parts in the session.  NX does not save the Disable Plane Translucency setting. 
For each session, it initializes the setting according to a customer default. 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: DESIGN
Version: V11.0.2
Function: FEATURE_MODEL

Ref: 001-9056922

KB Article ID# PL8003301

Contents

SummaryDetails

Associated Components