Mirrored Flatten views give the wrong value for Bend Orientation Callout

2021-10-06T23:51:33Z

Summary


Details

A flatten from a sheet metal file has been placed on a 2D draft. When a view is created from the other side of the flatten using the "Principal" view command, bend orientation Callouts give the same result when it should be mirrored. For example, a bend orientation will say "90°Up" instead of "90°Down". 



Solution

To restore the correct setting go to Solid Edge Options -> Annotation and check the option "Derive bend direction from drawing view". 

To update the views use: Ctrl + Shift "Update Views".

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DRAFT
Version: V110.0
Function: ANNOTATIONS

Ref: 001-8976777

KB Article ID# PL8003294

Contents

SummaryDetails

Associated Components