Network Locations cannot be set in managed Solid Edge options of ST8 on Windows 10

2021-10-06T23:51:32Z

Summary


Details

If you experience any of the following problems with ST8 MP11 on Windows 10:


  • Setting ST8 MP11 Insight Network Location in the Solid Edge Options failed with a local folder error.
  • Solid Edge does not open correctly upon start and must be restarted. 
  • If files are opened using the complete Insight managed http URL Path with read only permission, but they are shown available in the Sharepoint Insight Library. 

Then you should check if .NET Framework 3.5 feature is installed and activated in the Windows 10 Features.

Solution

To check the .NET Framework 3.5 feature, install and activate in the Windows 10 Features:


1. Select the Microsoft Windows Application Button with right mouse button 
2. Locate 'Programs and Features'. 
3. Access 'Turn Windows Features on or off '.
4. Look for .NET Framework 3.5 (includes 2.0 and 3.0). 
5. Toggle on the check box beside it and let Windows download and install.


After the installation all the problems should be resolved - if not please contact GTAC for further help.



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V108MP11
Function: INSIGHT

Ref: 001-9056755

KB Article ID# PL8003275

Contents

SummaryDetails

Associated Components