PMI note located in lower left corner does not keep its position when NX window is resized

2021-10-06T23:26:13Z

Summary


Details

Have a text that I want to show in the same size and at the same position regardless of zoom factor and/or the NX graphics window is resized.
Just adding PMI notes with default settings renders in text that slides around when NX window is resized and text size alters with zoom factor.

Solution

If you desire a constant size text in the lower right corner the following settings need to be applied to such text in Notes Settings menu:
- Display, Orientation group, enable "Display Parallel to Screen" and enable "Lock Size and Position"
In addition you need to set the desired anchor point for the text:
- Note menu, Alignment group, Anchor: Bottom Right  (Or for an existing text you could alternatively set it in the settings menu under Lettering in the Alignment group).



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: PMI
Version: V11.0.2
Function: NOTES

Ref: 001-9049689

KB Article ID# PL8003273

Contents

SummaryDetails

Associated Components