NX Templates Fail: ERROR: (641106) - Teamcenter Integration is not initialized

2021-10-06T23:26:13Z

Summary


Details

When attempting to install the NX 11.0 Templates to Tc10.1.7.1 using the 
command line: 
%UGII_ROOT%\templates\sample>tcin_template_setup.bat -u=infodba -p=infodba 
-g=dba


the ug_clone operation fails with the error:


----------------------------------------------------------- 
***** ug_clone import operation failed 
ERROR: (641106) - Teamcenter Integration is not initialized 
 while initializing import operation 
----------------------------------------------------------- 



Solution

During the Template import process, a 'nx_integration' is needed. 
In this case, the customer was licensed for an Academic bundle. There is no 
'nx_integration' license available for the 'infodba' user.


The customer's license file does have a 'TCUACAD' bundle that contains: 
'TCUACAD_nx_integration'. This bundle should be set for all users requiring 
NX CAD Integration. It also needs to be set for a 'dba' user who will be 
running the tcin_template_setup.bat.


To istall the NX Templates with tcin_template_setup.bat:


 1) Be sure that a 'dba' user has the 'TCUACAD' bundle set in the 'License 
 Bundle' field in Teamcenter Organization. 
 2) Open a Tc Command Prompt on a machine that has NX installed (2-tier).


 3) Run tcin_template_setup.bat with the 'dba' user's credentials. For 
 instance: 
%UGII_ROOT%\templates\sample>tcin_template_setup.bat -u=dba_user 
p=dba_user_pswd -g=dba


If installing on 4-tier RAC, Reference: 
 Document ID:002-7003616 - Upload NX templates thru 4Tier connection - 
 correction to 001-6351699 



Notes and References





Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V11.0
Function: STARTUP

Ref: 001-9045843

KB Article ID# PL8003268

Contents

SummaryDetails

Associated Components