Details
NX12 Mechatronics Concept Designer, MCD, fails to run simulation (Runtime error) while on NX11 this was
working.
When opening a model (perfectly working in NX11 MCD) into NX12 MCD, it gives
Runtime error when pushing the Play simulation button.
Object="Mainbody-FixedJoint(1)"
Owner Comp=6-003-000660
Desc=Attachment and Base are the same
Solution
An Object at subassembly level (6-003-000660) was used in higher level parent
assemblies and caused a circular reference.
NX 11 allowed the circularity, but NX 12 does not.
NX 12 is enhanced and report failing Object, Owner and Description.
Investigate and repair the possible circularity. This case by deleting the
Object (Mainbody-FixedJoint) in subassembly (Owner Comp=6-003-000660).
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: MECHATRONICS
Version: V12.0
Function: RUN_TIME
Ref: 001-9056653