'Show Grid' is turned ON, but the grid is not displayed

2021-10-06T23:26:13Z

Summary


Details

Even though the Grid Preference 'Show Grid' is turned ON, the grid does not display or is missing in the Drafting application.



Solution

  1. In NX9 Customer Defaults, expand 'Drafting' and highlight 'General'. 
  2. Select the 'Miscellaneous' tab. 
  3. There are 3 options for the 'Grid' setting: 
  •  Use Drafting Grid 
  • š Use Sketch Grid 
  • š Use Sheet Zone Grid 
In NX9, the 'Grid' setting could be set to 'Use Sketch Grid' or 'Use Sheet Zone Grid'. 
These settings will only display the grid if a Sketch is active, or to use the grid with sheet zones.


In NX11, this Customer Default is now under 
'Drafting-->General/Setup'-->Workflow (tab)'. In the 'Drawing' group, toggle the Grid Settings to the desired value ('Drafting', 'Sketch', or 'Sheet Zone'). 



Notes and References





Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: SETTINGS

Ref: 001-9055310

KB Article ID# PL8003251

Contents

SummaryDetails

Associated Components