Details
Using the Right Mouse button to create a new FEM and SIM is not working. The New Part File
dialog has this error msg:
There are no templates available to support the operation you are trying.
Either turn on the show blank templates customer defaults or add the templates
to the pax file to support this operation.
Solution
Examine the CAE pax file in a text editor, make sure the entry for ObjectData
class is set as:
ObjectData class="CaeFemTemplate"
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V10.0.3
Function: FILE_NEW
Ref: 001-9055275