Procedure for importing Teamcenter Table Templates

2021-10-06T23:26:12Z

Summary


Details

Procedure for importing Teamcenter Table Templates



Solution

Steps:


1. Ensure that the following environment variables are defined:


    - SPLM_LICENSE_SERVER


    - UGII_BASE_DIR


    - TC_ROOT  


    - TC_DATA 




2. Edit the "nx2_tceng_tables.clone" (available under "ugii\table_files") file to define if the location of each template part if it does not accepts "${UGII_BASE_DIR}\". Like below -


&LOG Part: "${UGII_BASE_DIR}\ugii\table_files\generic_table_english.prt"


Change to (Exact location)– 


&LOG Part: "C:\NX11\UGII\table_files\generic_table_english.prt"


Make these changes for other template parts files in the clone file.


For first template part the syntax will be like below in clone file-


*****************************************************************************


&LOG Part: "C:\apps\PLMx64\NX11\UGII\table_files\generic_table_english.prt"


&LOG Cloning_Action: DEFAULT_DISP Naming_Technique: DEFAULT_NAMING Clone_Name: @DB/generic_table_english/A


&LOG Container: "infodba:Tabular Note Templates"


&LOG Part_Type: Item


&LOG Part_Name: generic_table_english


&LOG Part_Description: generic_table_english


&LOG Associated_Files_Directory: "C:\apps\PLMx64\NX11\UGII\table_files\generic_table_english"


*****************************************************************************


3. Execute the Import utility (Note: This is a single line command)


Open TC command Prompt -


(Start > All Programs > Teamcenter 11 > tc_config1 Command Prompt)


Execute below command, like below (Check your installation location)


C:\NX11\UGMANAGER\tcin_import.exe -u=infodba -p=XXXXX -g=dba -l="C:\NX11\UGII\table_files\nx2_tceng_tables.clone"


4. Create the preview images for the template parts.


    - Login to Teamcenter as infodba


    - Start NX


    - Retrieve each template part and save part with preview enabled.  


(All the above templates will be available in Teamcenter at "infodba:Tabular Note Templates")
 
5.  Now in NX, go to Menu > Preferences > Palettes > Click on Open Palette > Browse for "tables_tceng.pax" file available under "C:\NX11\UGII\table_files" > Click OK


Now these Teamcenter Tables will be available under NX Resource bar to use.



Notes and References

9037464 

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0
Function: UTILITIES

Ref: 001-9037464

KB Article ID# PL8003228

Contents

SummaryDetails

Associated Components