Details
If user wants to monitor the operations performed in Plant Simulation, can Plant Simulation output/generate logs like syslog in TC or NX ?
What settings are required to enable log output and where it will be generated ?
Solution
As of now, there is no such functionality in Plant Simulation.
Hence there is no setting to enable it.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V13.0
Function: ALL
Ref: 001-9041742