Issues with indexing

2021-10-06T23:51:29Z

Summary


Details

Indexing options is only indexing a few files. In this case there were over 
2000 files and only 31 were being indexed. 



Solution

Before the folders and files can be indexed they must have the correct SYSTEM 
permissions:


- right-click the top level folder that is to be indexed and select Properties 
- select the Security tab 
- in the Group section look for SYSTEM 
- if SYSTEM exists make sure it has full-control 
- if SYSTEM does NOT exist Add it and give it full-control 
- in the folder Properties uncheck 'Allow files on this drive to be indexed' 
- in the folder Properties check 'Allow files on this drive to be indexed' 
- allow the changes to be applied to all subfolders 
- in Index Options click Rebuild



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110.0
Function: BUILT_IN

Ref: 001-9050836

KB Article ID# PL8003178

Contents

SummaryDetails

Associated Components