Solid Edge Direct Model at assembly level is not created from solid edge in TC

2021-10-06T23:51:28Z
ASSEMBLY

Summary


Details

Direct Model at assembly level is not created from solid edge in TC

Solution

It will not show the assembly dataset of direct model in TC.


This is correct behavior as it is allowed only create JT files of part, sheet metal and weldment files, but not assemblies.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2008
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V9.0
Function: ASSEMBLY

Ref: 001-9043093

KB Article ID# PL8003162

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS