Simcenter 3D Solutions Plotting a Nodal Displacement/Translation Using a Cylindrical Coordinate System But How Can Theta Have Inch Units?

2021-10-06T23:26:12Z
Simcenter 3D

Summary


Details

A Customer is running NX11.0.X, using Pre/Post, and doing SOL 601,129.  He's plotting a nodal displacement/translation using a cylindrical coordinate system.  He asks how can theta equal 1 inch?

Solution

This is working as designed.  Displacement - Nodal output is for only translation and not rotation.  Hence even for a cylindrical CSYS the displacement will be in linear translation units like mm or inch only. 

 

Displacement - Nodal in X will be shown as Displacement - Nodal, R where R equals the radial direction.  This will show the displacement of the node in the radial direction instead of using the X direction when a Cartesian CSYS is used. 

 

Similarly, Displacement - Nodal in Y will be shown as Displacement - Nodal, T where T equals the theta direction.  This will show the displacement of the node in the theta direction instead of using Y direction when a Cartesian CSYS is used.

Notes

Reference: IR 9041653 and IR 1781645.

KB Article ID# PL8003144

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow