Simcenter 3D Solutions Has Curved Polygon Face And Using Command From Polygon Face But Surface Is Flat.

2021-10-06T23:26:12Z
Simcenter 3D

Summary


Details

A Customer is running NX12, using Pre/Post and doing possibly SOL 101.  On a curved polygon face he executes the command From Polygon Face as follows:

https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_help/#uid:xid1128419:index_advanced:xid389662:xid1393939

However the resulting surface is flat.  He asks for an explanation.

Solution

This is working as designed.   The design doesn't take into account interior points on the face.  It only uses the boundary.  So, in the dialog here, we assume the user selected Surface.  That means the boundary of the polygon face is used to create a face (using N sided surface) in the part (.prt) file.  If you choose Boundary, then only the face edges will be used to create curves in the part file. 

 

In version 12, we have a new command that will generate a convergent body from a polygon body.  That command is Convergent Body from Body located in the Polygon Geometry group of the Home tab while in a .FEM file.  Here's the What's New article from the online help for the new command. 

 

https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_help#uid:index_whatsnew:xid1306881:xid1306885:xid1307297:xid1371248 <https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_help> 

Notes

Reference: IR 9043395

KB Article ID# PL8003143

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow