NX What is "APPLICATION_PROTOCOL" in new Export STEP dialog box

2021-10-06T23:26:12Z
NX for Design

Summary


Details

The NX 11's STEP Settings File contains a new setting - "APPLICATION_PROTOCOL" 
 What is this item used for?
 * ex) "APPLICATION_PROTOCOL=AP203" or so on

Solution

Since NX11 there is only one dialog box to export STEP file in all there formats. The format is chosen using the 'APPLICATION PROTOCOL' setting interactively. The same present in the setting file to identify. ==================================== 
The "APPLICATION_PROTOCOL" is set by the STEP export UI in NX at the time of execution. The settings file used is copied to a temporary settings file used for the translation being executed and the STEP export UI settings are added/overwrites the existing settings input at this point.
==================================== 

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V11.0
Function: STEP_AP214

Ref: 001-8969648

KB Article ID# PL8003115

Contents

SummaryDetails

Associated Components

CAD Translators