NX About vector editing of "Extrude"

2021-10-06T23:26:12Z
NX for Design

Summary


Details

During vector edit of extrude feature, in NX10 if a user would select a new face/direction, the old selection used to be deselected automatically. In NX11 user has to manually deselect the old face to change vector direction. (User thinks this as a problem)

Solution

This was a deliberate change. From NX11,  a vector can now be defined on a chain of faces rather than limited to only a single face. A consequence of this support is that the face selection is now multi-select, which means that the user must explicitly deselect faces if the intent of selecting another face is not to add faces to the chain.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V11.0.1
Function: FEATURE_MODEL

Ref: 001-8972078

KB Article ID# PL8003113

Contents

SummaryDetails

Associated Components

Modeling