Details
We are creating a JT file out of NX 9 and open it into our program. When we do
PMI notes are automatically displayed on the screen. Is there a way to not
create PMI in a JT file?
Solution
Yes if you go to <install_path>\NX 9.0\PVTRANS look for a file called
tessUG.config. Open that in a text editor and move to the ugConfig { section
at the bottom. There you will see many options for PMI that are set to False
by default, but since you are seeing PMI they are set to True. Set these back
to False and the PMI info won't be added to the JT file anymore.
Notes and References
Hardware/Software Configuration
Platform: AMD64
OS: window
OS Version: 764SP1
Product: NX
Application: TRANSLATOR
Version: V9.0
Function: NX_JT
Ref: 001-9041376