Simcenter 3D Solutions How to check energy transfered to the Fluid ambiant ?

2021-10-06T23:26:11Z
Simcenter 3D

Summary


Details

Customer define a thermal Heat Load to a Fluid domain (100W)

The fluid is in contact with the structuture.

Structure convect to ambiant fluid (air 20°C).

How to check energy transfered to the Ambiant Fluid? (100W)

Solution

+ Create a group with element free faces of the structure in contact with

ambiant fluid (gp1)

+ Create a Simulation Object type « Report Between Regions »

+ Primary Region :

select group gp1 (the gp created step before)

+ Secondary Region Override: Fluid Ambient

+ Thermal data: Heat flow

+ Solve

+ Open the Html report generated

« Linear Thermal Coupling » is the energy transfered to ambiant fluid=100W

this is the same value as input head load.

We can also check the NX Thermal log file:

begining of the file: « Thermal Boundary Condition »

input heat load of 100W

1 - Thermal Load(1) Heat Load 1.000E+08 mN-mm/s

Output:

At the end of the file we can find Summary for thermal elements:

Heat flow into sinks = 1.000E+08

Heat Flow+Load Summary Into Different Sink Entities:

Sink Entity Temperature Heat Energy absorbed

Fluid ambient group 2.000E+01 1.000E+08 0.000E+00

Notes

KB Article ID# PL8003061

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow