How to change the environment size in KeyShot?

2021-10-06T23:51:20Z

Summary


Details

How do you change the environment size in KeyShot? 



Solution

If your model is really large it might not fit the default environment size in 
KeyShot. To fix that you can either change the environment so it becomes 
bigger than your model or you can scale the model down to fit the environment. 
Here are the steps for each, using KeyShot 7:


To enlarge the environment: 
- Open the KeyShot file 
- Zoom out until you can see both the environment sphere and your model 
completely 
- Go to the Project Menu, Environment tab 
- Under the Transform pulldown, find the Size option 
- You can play with the slider or you can enter a number for the size of the 
environment. If the slider does not change the size enough, just enter a 
number in the field. That allows for any size independent of the slider scale.


To shrink the model: 
- Open the KeyShot file 
- Zoom out until you can see both the environment sphere and your model 
completely 
- Go to the Project Menu, Scene tab 
- Select the entire model by clicking the model name under the header Models. 
The whole model should highlight on the screen 
- Right below the box listing the models and cameras, there are three tabs. 
Click on the Position tab 
- Now use the scale slider or the scale numeric field to change the model so 
it fits the environment size. 



Notes and References





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: EXTERNAL_APPS
Version: V110MP3
Function: KEYSHOT

Ref: 001-9036884

KB Article ID# PL8003041

Contents

SummaryDetails

Associated Components