Fatal message (below) occurs on axisymmetric model. The geometry is properly
defined, but if we look inside the dat file, there is a node which coordinate
location is negative. It is practically zero, but has a very small negative
value (e.g. -1.0E-12). The problem is axisymmetric analysis doesnt allow
negative coordinate value at all.
*** USER FATAL MESSAGE 4660 (EQX4GC)
FOR ELEMENT WITH ID = 1000
THE GEOMETRY HAS NOT BEEN DEFINED PROPERLY. THE X (RADIAL)
COORDINATE MUST BE GREATER OR EQUAL TO ZERO.
^^^ USER FATAL MESSAGE 9031 (ERRPH1)
^^^ NOGO ENCOUNTERED IN SUBDMAP SEMG
Solution
Reduce the default accuracy of the Real Data Filter Value (e.g. from 1e-15 to
1e-10).
RMB on solution -> Edit Advanced Solver Options -> Formatting Options -> Bulk
Data -> Activate "Apply Real Data Filter To All Real Values" -> Modify Real
Data Filter Value (e.g. from 1e-15 to 1e-10).
Notes